Based on datasheet, TXS02324 support for 3G. then does it also support for 4g?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Based on datasheet, TXS02324 support for 3G. then does it also support for 4g?
Hi,
I am not sure on the protocol requirements for 4g. As you see, the datasheet was last updated in 2011 so that is why it doesn't mention 4g.
Thanks!
-Karan
the requirement is 100 Mbit/s and can also reach 1 Gbit/s. But how about TXS02326? does TXS02326 can support with 4G?
Hi,
Our auto bidirectional translators are limited to under 100MHz of operation. So it seems like it will not support your application.
Thanks!
-Karan
can you give us recommendations for your bidirectional translator products that meet these requirements? please
There is no requirement for 100 Mbit/s or 1 Gbit/s. The communication between the phone and the base station has nothing to do with the interface between the phone and the UICC.
ETSI TS 102 221 V16.0.0 (2019-07) says:
5.1.4 Clock CLK (contact C3)
The terminal shall support 1 MHz to 5 MHz.
Not coincidentally, the TXS02324's specified fmax is 5 MHz. So it supports modern SIM cards just fine.
The TXS02324 handles only the electrical part of the SIM card interface. This has not changed for 4G/5G.