This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is checking with me a replacement. they used to use 74VHC14MX from fair child. but they need a upgraded device to handle a 40M 5v input signal,but the output is 3.3V . I found SN74AHC14 is a close one to 74HC14MX, but the Tpd is just the same level. would you please recommend a better device for this case? thanks. BTW, drop in replacement is better, TSSOP(14) package.
Fairchild's VHC and TI's AHC are pretty much equivalent, and support 70 MHz at 3.3 V.
There is no faster drop-in replacement. For different packages, look into the LVC family (e.g., 2× SN74LVC3G14).
What is the problem with the 74VHC14MX? Does it not handle the 40M signal? What is the output load capacitance?
Hi Yue,
The SN74AHC14DR would be an exact drop in replacement. If you want a TSSOP version, then you can go with SN74AHC14PWR. You can also check out the SN74LVC14APWR.