Part Number: SN74AXC4T774
Other Parts Discussed in Thread: TXB0104
Hi,
I have a question for the bidirectional Level translator SN74AXC4T774 when there is a bus contention:
The connection is shown as below:
FPGA --- SN74AXC4T774--- Unknown DUT
SN74AXC4T774 Setting: Direction from FPGA to DUT.
FPGA set: output data =0.
DUT set: output date =1. (for 3.3V)
As a result, the level translator's output will be pulled down. The 3.3V from DUT will be shorted to GND.
As I know about the SN74AXC4T774, there is a idea to add a series resistor of 150 ohm to limit the current below 25mA, it is safe for AXC device.
For normal operation, the drive strength of the FPGA is 12mA, also for the DUT. This is OK.
But, there is a worst case, the DUT is unknown for different products. A broken DUT can be short to 3.3V power supply. Therefore, the 150 ohm is useful to limit the current.
However, this IO is used for high bandwidth >50MHz. Thus, the RC is important. With 150ohm and 20pF, the cut frequency is 53MHz. The capacitance in the circuit is >50pF.
It is not preferred to add a resistor in this chain.
Do you have any idea to protect the bus contention without the series resistors?
Thanks.