This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN10KHT5541: ECL to TTL Logic: Going from Differential to Single-ended Inputs

Part Number: SN10KHT5541


I'm looking at the SN10KHT5541 as a component to use as part of my circuit. My circuit involves translating NIM-logic signals (essentially fast current-based logic, MECL). You can find the logic standards at the NIM wikipedia page:


https://en.wikipedia.org/wiki/Nuclear_Instrumentation_Module

This is based off of a reference circuit which utilized the MC10H125 ECL to TTL converter by OnSemi.

https://www.onsemi.com/pub/Collateral/MC10H125-D.PDF

http://www.hephy.at/project/electronic2/__PDF__/Translator/TTL_NIM%2520user%2520manual_v10.pdf

Now, going from a differential input to a single ended input, I was wondering what kind of considerations one must take? Are there some example circuits that may be able to provide some guidelines as to how to work with the SN10KHT5541? Also, regarding the OE pins on the SN10KHT5541, they look to be inverted, so do both pins have to be asserted to GND (logic low) in order to make sure that the IC is active? Both pins are the same functionally, but one is meant for ECL signals and the other is for TTL logic voltages, correct? Do both of them have to be asserted for the IC to be active, or should I just connect only one of them to GND (the TTL OE pin)?

  • Hi Jason,

    Just make sure to follow the provided specs in the D/S and maintain a good layout around the device. Unfortunately, I don't have an example circuit for you.

    Here is how the two OE pins can be operated:

    Yes one is meant to be controlled with ECL and the other with TTL. If either goes High, the output will be disabled so you can leave one of them grounded and just operate the other.