This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T245: VCC isolation

Part Number: SN74AVC4T245

Hello,

I'm running into an issue on a handful of boards where when one of the VCC rails goes low (VCC isolation event) the SN74AVC4T245's second power rail pulls ~100uA-400uA more current.

In this case, we bring VCCa to 0V (which is also tied to OE) and the VCCb side is still high. We see an additional ~100uA-400uA pulled from our battery and removing the SN74AVC4T245 stops the issue from occurring. We have 2 SN74AVC4T245's on our board but only 1 sees this issue and its not consistently the same device. 

Its my understanding from the datasheet that if one power rails goes to 0V that the outputs should go high impedance and the device should pull no more than ~5uA, is that correct?

If not, how much current should we expect to see during this situation?

Thanks,
Nick