Other Parts Discussed in Thread: TXS0101, LSF0101
Dear *,
please can you suggest a bidirectional level translator from 3V3 to 1V8?
The Ethernet phy is 3.3V and the application processor is 1.8V .
Signal is WAKE, type T/s (Tri-State is a bi-directional, tri-state input/output pin.) , Bi-dir.
When Wake signal then is this pin output from ETH_PHY, when OBFF mode (Optimized Buffer Flush/FILL) then i assume it is input to ETH_PHY.
Best Regards,
D.