Other Parts Discussed in Thread: SN74AXC4T774, SN74LVC1T45
Hi,
As shown in the datasheet of SN74LVC1T45-Q1.
"In a bidirectional application, these enable times provide the maximum delay from the time the DIR bit is switched until an output is expected. For example, if the SN74LVC1T45-Q1 initially is transmitting from A to B, then the DIR bit is switched; the B port of the device must be disabled before presenting it with an input. After the B port has been disabled, an input signal applied to it appears on the corresponding A port after the specified propagation delay."
As we can see, there is no ENABLE pin of SN74LVC1T45-Q1.
What you means the B port of the device must be disabled before presenting it with an input? How can you disable the port?
Is it the same as SN74AXC4T774, make sure the B port is no signal or floating during the direction change period?