Part Number: SN74HC595
Due to a circuit failure with a SN74HC595 shift register in circuit, an engineer measured the input resistance of a "good" similar IC between the "SRCLR"(not) and the "SRCLK", pins 10 & 11 respectively, with
a Keysight "micro-ohm" resistance meter. This was measured from pin 10 to 11, i.e. pin-pin, in a no Vcc applied environment.. Later he realized that the meter at the very low resistance scale was applying an 11.3V potential to the paired pins when the input resistance measured was near 800k ohms. So the question is, given the meter applied voltage was the IC stressed in any manner that would possibly cause a reliability issue over time? Again, no Vcc was applied to the IC at the time.
Thx in advance.