Part Number: SN7416
Please help me with the SN7416 Hex inverter buffers / drivers with high-voltage outputs for gate driver. How to use this IC for driving my IGBT (+15V and -9V)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This device cannot be used for -9V operation. All buffers available in the logic portfolio are meant for digital signals which go from a positive voltage to GND.
Thanks!
-Karan
Can you send me some typical schematic so that i can use this Ic as my input buffer to drive my IGBT. can i leave some channels floating or pulling them down through resistor. As i need two channels for totem pole operation.
Thanks
Geet