Part Number: TXB0104-Q1
My customer asks:
The TXB0104-Q1 is used for SPI voltage translation. In the datasheet,SCES727A the typical application schematic diagram shows the System (Master) Controller is connected at Port-A and the driven device (Slave) is connected at Port-B.
What if the Master Controller (5V) is connected at Port-B and the Slave - at Port-A (3.3V)?
Is this possible?
BR Josef