Part Number: LSF0102
Hello,
The video on single supply translation says, "The supply used must be at least 0.8 V larger than the lowest desired translation voltage."
Q) Is this lowest desired translation voltage referring to Vref_A?
It also says "The voltage of Vref_A must be selected as the lowest voltage to be used in the system."
Q) Vref_A can also be lower than the lowest signal voltage correct? For example if I'm translating between 3.3 and 1.8, can Vref_A also be 1.5 V?
Thanks,
Vibhu