This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104-Q1: When unused pin is open

Part Number: TXB0104-Q1


Hi team,

What happens if unused pin is open for both side? A customer didn't tie it to GND by mistake. I refer to some comments like below in E2E, but can you explain more easily?

"Unused IO pins for the logic devices are advised to be connected to gnd, however, the TXB is like a weak latch which tries to maintain a defined high or low state."

In addition, is it possible to connect directly the unused port to GND without pull down (100kohm)? Otherwise, does it have to use pull down resistor?

Thanks,

Sam Lee