Part Number: CD4081B
Other Parts Discussed in Thread: SN74LVC1G08
Hi:
We have used the CD4081B AND Gate in a design and we have a doubt with the Output High (Source) current.
Every 5 secondos, during 3 milisecons, we need a 4,7mA output high current in a Output. We can see that the output voltage goes down from 5V to 3,5V. It is because the output current in the output is to high and the component can not give the power we need.
For the circuit that we have design, the 5v to 3,5V drop voltage is correct, but we would like to know if these operating mode for the CD4081Bis correct. We would like to know if the CD4081B is working in a degradated mode an we are decreasing the live of the component.
Thank you