Other Parts Discussed in Thread: LMK00804B-Q1, SN74LVC1G34
Hello,
My goal is to to translate 2.5V logic level (from MAX10 FPGA) to 1.8V logic, driving a 50ohm load.
It means that I need a device capable of driving 1.8V/50ohm=36mA.
I didn't find any device capable to drive such current, so my question is:
1. Can you recommend about a device like this?
2. do you recommend using few devices (or one dual/quad..) by connected inputs and outputs in parallel, to increase drive capability? (As mentioned in https://e2e.ti.com/support/logic/f/151/t/437301?Suggested-Logic-Buffer-for-driving-TTL-50-ohm-load)
3. Is it possible to use a Clock buffer (like LMK00804B-Q1), which seems to be capable of driving 50ohm loads?
Thanks!
Max