Part Number: TXB0106-Q1
Hi team,
I have 3 questions below for TXB0106-Q1 use case.
1) I plan to use 1.8V - 3.3V level translation. 3.3V power up first and then 1.8V rail power up.
Is that OK to directly connect 1.8V rail to OE pin? I placed 1Mohm resistor, but now I am considering to remove it.
2) It is recommended to place external pull down resistor in the datasheet. Is there any internal pull down resistor?
If yes, how much is the value?
3) Is there any restrictions in power down sequencing for OE pin? for example Must pull OE pin Low before Vcca/Vccb shut off?
regards,