Part Number: SN74AHC08
Hi team,
As the thread you reply in below, the SN74AHC08 is with Schmitt trigger input and the range is 200mV.
But still confuse that from your post, when VCC=3V, VIL and VIH are 1.5 and 1.7V.
In the SN74AHC08 datasheet, VIL and VIH are 0.9 and 2.1V and between 0.9~2.1V, they are unknown or they are Smitt trigger range since I cannot see the spec from the datasheet?
https://e2e.ti.com/support/logic/f/151/p/852977/3154580#3154580
Also, for the SN74AHC08 operated as below conditions and waveforms as below pictures.
You can see Y is oscillate.
Does that cause the SN74AHC08 damage if usually under the conditions even that's no over absolute max rating?
VCC=3.3V
A is yellow waveform (SR is less than the datasheet max value), B is 3.3V.
Y is blue waveform.
Thank you!