This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV02A - ICC Max Current 5V - 20Ma



After setting up a test to monitor the current (ICC) at 85 degree's C, having the inputs terminated, with six devices the total current draw is ONLY 500nA at 3.3V power. To calculate the battery life of the product is this an anomally or is there a 'Typical' value that TI can provide? The ICC max is identified on page  3 of the datasheet;

at 5V Max = 20uA.

Since there is such a large discrepancy between the test results and the Max current listed, I wanted to verify and possibly get a typical value to make the best battery life calculations.

-Tom-