Part Number: TXB0104-Q1
Other Parts Discussed in Thread: SN74LVC2T45-Q1, SN74LVC1G17-Q1
Hi team,
Can you confirm if TXB0104-Q1 is okay for SPI interface of below configuration?
Thanks,
Sam Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0104-Q1
Other Parts Discussed in Thread: SN74LVC2T45-Q1, SN74LVC1G17-Q1
Hi team,
Can you confirm if TXB0104-Q1 is okay for SPI interface of below configuration?
Thanks,
Sam Lee
This will work, if the traces are not too long and if there aren't any strong pull-up/-down resistors.
For unidirectional signals like these, are more robust solution would be to replace the TXB with unidirectional or direction-controlled translators, e.g., SN74LVC2T45-Q1 for uptranslation and SN74LVC1G17-Q1 for downtranslation. (For 5 V, there is no such translator that does both in a single device.)
Shouldn't there be some chip select signals?