Other Parts Discussed in Thread: TXB0108, , SN74AXC8T245
Hi,
To give a brief introduction, we are testing an ADC chip which outputs data at 1.8V. We are using KC705 board with its FMC XM105 Debug Card to gather the data from ADC's EVAL board. KC705 has IOs operating at 2.5V so we had to deploy a level shifter (TXB0108) in the design before the interfacing connector. Unfortunately the interface altogether generated capacitance >70pF which caused ringing on data lines. Now we are in the process of revising our design to cater the ringing and decided to add a line driver(SN74ALVC244) between the interface connector and the level shifter.
We want to know :
1. What is the total current consumption of SN74ALVC244 operating at 2.5V?
2. What value(s) of decoupling capacitors should we place on TXB0108 and SN74ALVC244 with data lines operating at 3MHz and with interface creating capacitance >70pF?
Thanks,
Justin