Hi team
My client wants to realize two-way signal level conversion through one buffer or two buffers:
1. First signal: Vin 3.3V conversing to Vout 5V.
second signal: Vin 5V conversing to Vout 3.3V.
2. The maximum frequency of two signals can be 20 m, so the customer is worried that two high-frequency signals in the same buffer will cause EMC problems and interference.Do we have the design or model of buffer for high frequency signal and EMC interference like this?
3. I haven't found the GPN of buffer which is open-drain output with Schmitt-Trigger, could you please help me double-check that?
Best Regards,
Wesley Huang
Email: wesley-huang@ti.com