Is there an open drain buffer/device that has schmit trigger CMOS input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an open drain buffer/device that has schmit trigger CMOS input?
Hi Emile,
Clemens suggested implementation will work for this. It is true that the recommended max is VCC however the abs max for output voltage in the high impedance state is 6.5 V. The issue that could arise if you do plan have the output go above VCC is if somehow the output drives high then current can conduct through the parasitic diode of the pfet. If the inputs are tied low and the pull-up value is large (~10kohm), this shouldn't cause much concern.