This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G332: sn74lvc1g332dbvr v 74lvc1g332dbvrG4

Part Number: SN74LVC1G332


Hi,

I have a CM asking me about the two parts in the title.It looks like they are form fit and functional equivalent with the only difference being the lead/ball finish - is that true?

The G4 has the lead/Ball finish - CU NIPDAU

the SN74 part has these two options CU NIPDAU | CU SN - from note 6 in the datasheet it looks like these are two mutually exclusive lead/ball finished - is tat true? - and if so how do I know what part I get?

Cheers

Calum