Part Number: SN74AUP2G07
Other Parts Discussed in Thread: SN74AXC4T245, SN74AXC2T45
Hello experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AUP2G07
Other Parts Discussed in Thread: SN74AXC4T245, SN74AXC2T45
Hello experts,
The SN74AUP2G07 would work. Its outputs are limited to VCC + 0.5 V only when the they are active; in the high-impedance stance, you are allowed to pull them up to a higher voltage.
If you want to shift 1.25 V input signals to 3.3 V, then you should use a level shifter like the SN74AXC4T245. Is it necessary for the outputs to be open-drain?
Hi expert,
Hi Shreyas,