Part Number: SN74LVC1G17
HI Team,
There is not any TYPICAL data for Electrical Characteristics in datasheet, including VT+, VT- . My customer need these typical data. Could we provide them?
Thanks,
Garrick Dia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G17
HI Team,
There is not any TYPICAL data for Electrical Characteristics in datasheet, including VT+, VT- . My customer need these typical data. Could we provide them?
Thanks,
Garrick Dia
Hi Garrick,
The typical char are not guaranteed and depends on the device PVT specs ( Temp is usually 25C for typical values). What is guaranteed by the datasheet is the min / max specs only.
Why does the customer require the typical char and what are the test conditions? I can try to look if we have the data.
Please check these typical data under room temperature. Customer need them for circuit design calculation instead of using max or min. Thanks.
Hi Garrick,
I found the typical data for 2.3V and 4.5V Vcc below:
1.38 V VTP_2p3V 780.000 mV VTN_2p3V
2.47 V VTP_4p5V
1.67 V VTN_4p5V
To reiterate, this is not guaranteed for all the shipped out devices from TI and min/max on datasheet is to be considered while designing.