Other Parts Discussed in Thread: SN74AXC4T774
We have noticed, that in our design the VCCA of the TXB0106 level translator is connected to +2.5V power supply and SPI interface signals and VCCB is connected to +1.8V supply and interface signals (see the attached picture). The interface is functional, but the supplies do not meet the datasheet's specification for VCCA =< VCCB.
My question is, will there be some consequences for the level translator in this case e.g. will the level translator fail in long term or in high/low temperature or is there current flow from VCCA to VCCB or are some other issues possible?