Part Number: TXS0104E
Hi,
I would like to know if the TXS0104E device supports Vcc isolation feature (Ioff)? What would be the status of the I/O ports when VccA=0 and VccB=3.3V? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Naig,
This part does not have the Ioff. You can verify this by looking into the Electrical Characteristics table and you should see a spec labeled Ioff if the device has that feature. There's no guarantee what the status of the I/O are for devices without that feature when the supply is at 0 V.
I understand there is no Ioff feature. How about the information stated on this post by Emrys Maier? https://e2e.ti.com/support/logic/f/151/t/641497?TXS0104E-OE-pull-down-resistor-value
Isn't reliable that when either supply is at 0V, all I/O will be high impedance?
Hey Naig,
It's likely that the I/Os do go into a high-impedance state when one of the supplies is at 0 V, but since there is no Ioff spec (this isn't tested) this can not be guaranteed.