Other Parts Discussed in Thread: CD74HC4046A
Hello everyone,
We are working with the PLL to boost a 60 Hz signal up to a signal that oscillates 2^18 times faster, roughly 15.728 MHz. The input signal can vary from about 40 Hz to 70 Hz, so the output from the PLL needs to have a range of about 10 MHz to 20 MHz.
We've had trouble getting the output signal to the right frequency. Currently it's at 400 kHz, which appears to be the minimum offset frequency. The person who designed our PLL is looking into the correct resistor and capacitor values for R1, R2, C1, R3, and C2. But I've also been doing some research since we can't really move forward until this is resolved. We've tried a couple different combinations, but nothing has gotten us into the MHz range.
I've looked a lot at the App Note for an older generation of the PLL (http://www.ti.com/lit/an/scha003b/scha003b.pdf). However, I've haven't worked with a PLL before, so I'm struggling to grasp what size resistors and capacitors we need. Also, since this older PLL seems to rely on higher voltages, I'm concerned that some of the documentation doesn't really translate to the newer part.
Does anyone have any insights into what values I should use for the resistors and capacitors? Or is there another reference I could use that might help?
Thanks,
- Tom