Hello,
I am looking for a part for MII, RMII and RGMII interface voltage translation between 1.8 V - 3.3 V, up and down translation. Uni-directional is okay.
Requirements:
- < 10 ns max delay between input and output pins
- < 10 ns delay difference part to part
- < 1 ns delay skew channel to channel
Here are my questions:
- It looks like for my voltage range the part meets requirement 1, can you confirm 2 and 3?
- Do the propagation delay values in 6.11, 6.12 and 6.13 also account for requirement 2?
- Is there a specification on the datasheet for requirement 3?
- Is there a part that would be better suited given the application and timing requirements?
Thanks,
Vibhu