Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not Gate Logic

Other Parts Discussed in Thread: SN74AHC540, SN74AHC16540, SN74AHC240

Hi,

I am looking for a chip which would act like a "NOT Gate".

Requirement is: I have two select lines wherein i want to select either of the 1 between 2. So when 1 pin drives to VCC other would drive to 0V. It would be good if a chip has array of NOT Gates. High on line-> 2V to VCC. VCC i am good with 3.3V - 5V.

Please suggest suitable part for this.