FAQ: Logic and Voltage Translation > Monostable Multivibrators >> Current FAQ
The application report Designing with the SN74LVC1G123 Monostable Multivibrator has some useful information regarding this.
Essentially, the timing is primarily determined by the external resistor and capacitor on the board. These components usually have very large variation over temperature which will be of much more concern than the variation from the monostable device itself. The above app note shows that, when isolated, the temperature change of the monostable multivibrator device will result in less than 1% variation in the output pulse width. It is relatively common to see a capacitor's value vary 25% or more over temperature, which will directly translate into error in the pulse width for this type of device.