This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: PCIe Wake# and CLKREQ# ISSUES

Part Number: LSF0204


Hi,

I’d like to know which item Bidirectional bus buffer gate can design in pcie 3.3V Wake# and CLKREQ# signals.

The LSF0204 can use in 1.8V to 3.3V only, we need 3.3V to 3.3V to extend Wake# and CLKREQ#.

In PCIE SPEC, Wake# and CLKREQ# are defined for Bidirectional

 

Best Regards

 

perry

 

 

  • The LSF is a passive switch; it cannot buffer the signals.

    And it is not possible to have a bidirectional buffer without a direction control signal, because when the voltages at the two sides are different, the buffer cannot know which one should override the other.