Part Number: TXS0108E
Other Parts Discussed in Thread: SN74LVC245A, SN74AXC8T245
Hello
can i use the part TXS0108EPWR as a buffer by giving both vcca and vccb 3.3v,i want this as bidirectional transceiver
Regards
babu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0108E
Other Parts Discussed in Thread: SN74LVC245A, SN74AXC8T245
Hello
can i use the part TXS0108EPWR as a buffer by giving both vcca and vccb 3.3v,i want this as bidirectional transceiver
Regards
babu
By definition, the auto bidirectional translators are weak buffers in order to allow the input signal to over drive the present state.
The TXB is weak buffer providing 20uA of DC drive strength; ideal to interface high impedance loads.
TXS have internal FET with pullup resistors on both sides for allowing voltage level translation. The oneshot circuitry provides momentary AC drive on both TXS and TXB.
Hello shreyas
thanks for the Reply
can you please suggest any part with bidirectional or auto directional tranciever with 3.3 level ,main aim is to use it as buffer at 3.3v with 8 i/o
A transceiver with a direction input is the SN74LVC245A.
A transceiver with automatic direction sensing does not exist, and cannot exist.
You could also consider using the SN74AXC8T245 which can work as buffer with 3.3V on either sides.