This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: We are looking for solutions to replace PI4ULS5V106.

Part Number: LSF0108


Hi team,

We are looking for solutions to replace   PI4ULS5V106.

key requirement:

voltage range:1.05V - 3.3V

channels: 6 channels bi-direction, no DIR pin.

frequency>50Mhz

small package

Feel free to share your recommendations.

Thanks.

  • Frank,

    LSF0108 would be the best suggestion against the requirements shown. Its not a P2P solution as LSF0108 is 8bit vs Pi4UL is 6 bit solution, but the architecture and functionality of both are the same. To achieve 50Mhz, strong pullup resistors and low capacitive loading are recommended.