Part Number: CD4503B
Other Parts Discussed in Thread: CD40109B
Hi Friends.
I have a small doubt.
If the VDD pin is connected to +12V, is it possible to switch the output Q1 by providing 0 and +3.3V at the input D1
In the circuit given I am using the buffer CD4503B, the GPIO is switching at 3.3V logic is it possible to control +12V at its output level using 3.3V at the input provided the DISABLE pins are connected to ground directly.