This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G97: SN74LVC1G97DBVR will work on 5V or not or should we use a level translator.

Part Number: SN74LVC1G97


Hi,

We are using SN74LVC1G97DBVR, the VCC voltage applied is 3.3V. We are using it as an AND gate. One of our input is 5V. As per the datasheet it supports input voltages upto 5.5V.

Please help us to understand whether it will work on 5V or not or should we use a level translator.