Hello,
Your website says the SN54HCT244-SP is a space component. I don't see what krad rating the component has. Could you please point me to where I can find this information?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Your website says the SN54HCT244-SP is a space component. I don't see what krad rating the component has. Could you please point me to where I can find this information?
Thanks,
Hi Juan,
This part doesn't have a RHA.You can go to the order now section of the product folder to see the OPN. You will see that this device comes in 2 part numbers:
5962-8513001VRA and 5962-8513001VSA
Referring to the following FAQ on part numbers:
3056.3872.DLA Standard Microcircuit Drawings (SMD) and JAN Part Numbers FAQ.pdf
5962 refers to the Federal Stock Designator, - implies no RHA, 85130 is the drawing designator, 01 is the device type, V is the device class which is defined in the FAQ, and the last two letters, SA or RA refer to the package type.
You can also review these slides on the process flow and nomenclature of the HiRel parts.

Thanks!
-Karan