This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G373: LE pin overshoot

Part Number: SN74LVC1G373


Hi,

My customer found overshoot on LE pin at D pin Low to High.

Please refer the following waveform.

(CH1; LE, CH2; Q pin)

At they change D pin Low to high, and Q pin become low to high. LE pin has overshoot.

Do the device have any problem?

Vcc=5V

D pin is pullup to Vcc with 100kohm.

Thanks

Muk