This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: Issue interfacing this part to SD Card (level translating b/w 1.8V and 3.3V)

Part Number: TXS0108E

Hi,

I am using TXS0108E as level shifter between host FPGA and SD Card. I observed an issue in the response from SD card for CMD8 during SD card initialization. When I probed the CMD line on both the sides of level shifter I see that the host side CMD line is not tracking SD card side CMD line at some point.

I have checked with Xilinx and Trenz and they do recommend using SD-card specific level translator. However I didnt understand the reason behind it and why it is failing with TXS0108E.

Any reason on why this is failing and any further debug suggestions are really appreciated.

-

Mohan.