Part Number: LSF0108
Other Parts Discussed in Thread: TXB0108, SN74AXC4T774
i want to conversion the SPI signals' s level from 1.2V to 3.3V, the LSF0108 requires both 1.2V and 3.3v need to pull up, but the spi_EN need to pull down and connect to GND ,how should i do to meet the requirements of conversion the spi_EN's level and pull down to GND at the same time.
Meanwhile, can i also need to make other spi signals pull up to 1.2V or 3.3V use the 4.7K resistance when i alreaday pull up them to 1.2V and 3.3V in the lsf0108 side ?
Thanks very much.