This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC16T245: SN74LVC16T245

Part Number: SN74LVC16T245


Hi, Ti experts;

we are using SN74LVC16T245;

The data sheet describes the Ci of shared port pin values 4pF typically.

My customer wants to know how to test the Ci, and can i use the LCR to test?

if we can use LCR to test , how should the test conditions at measuring the Ci be set?

Thank you very much for your help!

Best regards

  • Hi,

    The input capacitance can be measured by providing an AC signal to the input and measuring the input current to find the input impedance.

    Capacitive impedance is 1/(2*pi*f*C). I recommend inputting an AC signal at 10MHz and measuring the input impedance.

    Thanks!

    -Karan