Part Number: TXS0102
Other Parts Discussed in Thread: TCA9800
Team,
my customer uses TXS0102 to convert 1.8V I2C signals to 3.3V I2C signals (I2C_SCL, I2C_SDA).
The I2C master is an FPGA. There are 3 slaves connected to the TXS0102.
The low-levels are
- 0.5V with external 2.2kOhm pull-ups
- 0.4V without external pull-ups
Are those (relatively high) low-levels normal for TXS0102?
I see a comment in the datasheet that this device is meant for point-to-point topology.
Could the 3 slaves be causing this behavior?
Thanks!