Part Number: SN74LVC1G125
Other Parts Discussed in Thread: SN74AUC1G125, SN74LV126A
Hi,
I'm looking for the 3-state buffer which delay time is shorter than SN74LVC1G125DCKR and pin-compatible device. Do you have recommend device?
Regards,
Nagata.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G125
Other Parts Discussed in Thread: SN74AUC1G125, SN74LV126A
Hi,
I'm looking for the 3-state buffer which delay time is shorter than SN74LVC1G125DCKR and pin-compatible device. Do you have recommend device?
Regards,
Nagata.
Hi,
For another topic, I'm looking for the TI part for TC74LCX125FK.
Condition are :
- Pin compatible with TC74LCX125FK
- Vdd range = 3.3V ~ 5V
Regards,
Nagata.
The SN74LVC1G125A is not available in the VSSOP package. (TI uses VSSOP only for Little Logic devices.)
Hi Nagata,
Unfortunately TI does not offer a buffer that is exactly pin compatible with this device.
However if the pin compatibility becomes non-issue, the SN74LV126A might suit your needs.
Thanks!
Chad Crosby