This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74AC00: More Outputs = More Output Current?

Part Number: CD74AC00
Other Parts Discussed in Thread: SN74HC00, CD74HC00, SN74HC374, CD74HC374, SN74AC00, , SN74AC374, CD74AC374, 74AC16374

Does an 74AC (or 74HC) series  IC have a  greater Vcc or GND current rating if it has a larger number or outputs i.e. a 74HC00 quad NAND gate IC has 4 outputs and +-50mA (100mA for 74AC00) Vcc&GND current rating-- does that mean that  a 74HC374 8-bit wide latch has a +-100mA Vcc&GND current rating (thus presumably 200mA for 74AC374) since it has 8 outputs?  

Thanks for any help!