This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: ADC values reading inaccurately after passing through TXB0108

Part Number: TXB0108
Other Parts Discussed in Thread: ISO7842, SN74LVC2T45

Hello,

I am passing a MISO line from an 16bit res adc (LTC2326) through the the TXB0108 in order to transition from 5V to 3.3V. I have slowed down sampling to 1per second so its not a speed issue. 

Unfortunately the values that I read are all over the place and inaccurate. When I read the values prior to the going through the TXB0108 I read correct values. I have even put the 5V signal through a resistor divider and even that works. It has to be something with the TXB0108. 

Am I missing something here? OE is held at 3.3V. 

Thanks so much,

Will