Part Number: LSF0101
Is there a Spice model available for these parts?
If not, then is there a parameter set for the internal MOSFET so I could kludge my own?
My design has VREF_B at 3.3V. The other side will be varied by the application per the customer's spec. The range of the "A" side is 1.8V to 3.3V. At the 3.3V level on "A", there is not enough difference between "B" and "A". Using the app note, I formed VREF_A from a resistor voltage divider derived from 3.3V. I set the VREF_A voltage at 1.5V . Seems like it will work, but I would like to have simulation examples to prove to the rest of team that the solution is viable.
Thanks.