This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ALVC244: Can SN74ALVC244 used in Hot insertion application

Part Number: SN74ALVC244
Other Parts Discussed in Thread: SN74ALVTH162827, SN74LVTZ244

I had a question about SN74ALVC244. Does it have diode to GND or VCC on the pins? In a hot swap application, (  Most of logic IC s has internal diodes at supply and GND can handle 10mAmp current ) I want to keep the backplane signals tri-stated until the board powers up. I am using this device to isolate and achieve this requirement. Is this device suitable for this use case?

Another similar application uses SN74ALVTH162827. Are they both similar devices?