This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC1G08: SN74AUC1G08 working at 3.3V

Part Number: SN74AUC1G08
Other Parts Discussed in Thread: SN74LVC1G08

Hello Team,

the SN74AUC1G08 can operate as abs. max at 3.6V while the maximum recommended voltage is 2.7V.

I'm not expecting any problem by operating the part by 3.3V continuous.

I think the only drawback would be that none of the datasheet parameter is qualified/tested up to 3.3V but rather 2.7V.

  • Can you confirm it?
  • Do we have alternatives to the SN74AUC1G08 that have datasheet parameters tested up to 3.3V?

Thanks,

SunSet