Part Number: TXB0104
Other Parts Discussed in Thread: SN74AXC4T245
Dear Team,
Do we have P2P TXB0104RUTR device and have a higher driving current?
If no P2P, please also suggest a higher driving current devices.
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0104
Other Parts Discussed in Thread: SN74AXC4T245
Dear Team,
Do we have P2P TXB0104RUTR device and have a higher driving current?
If no P2P, please also suggest a higher driving current devices.
BR
Kevin
To make automatic direction sensing possible, the TXB necessarily has weak output drivers in order to allow other devices to override the voltage level.
What is the actual problem you're trying to solve? Do you actually need automatic direction sensing?
Dear Ladisch,
Thanks for the input.
They use it for level shift for MAC, let me check with them if the automatic direction is necessary or not tomorrow.
In the meantime, do we have non-automatic P2P and stronger driving device?
BR
Kevin
Hi Kevin,
Unfortunately nothing that we offer that's direction controlled will be P2P; however, I have some part recommendations:
The SN74AXC4T245 is our new line of bus transceivers (level shifters) and has a much higher drive strength at the output.
If you're looking for something that has a higher supply voltage rating (and a little higher drive strength), then the LVC family will be better, but we don't offer any 4-bit devices from that family.
Thanks!
Chad Crosby
I guess you are using (R)(G)MII? Which one?
(As far as I can see, all lines except MDIO are unidirectional.)