Part Number: SN74HC595B
Can 4 of these devices be connected "in series" to provide a 32 bit output? If so how?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HC595B
Can 4 of these devices be connected "in series" to provide a 32 bit output? If so how?
The logic diagram shows that all eight shift register flip-flops share the same clock signal, and that the output of each flip-flop connects to the data input of the next flip-flop in the chain. (Whether this is a single Data input or separate Set/Reset inputs does not matter.)
To cascade multiple devices, do the same: route the same clock signal to all SRCLK inputs, and connect the output of the last shift register flip-flop (QH') in each device to the data input of the first flip-flop (SER) in the next device.
Typically, you would also want to share the SRCLR and RCLK signals.