This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T245-Q1: Slew Rate

Part Number: SN74AXC4T245-Q1

Hello, 

Is it possible to request for the slew rate at the following conditions?
VCCA 1.2V to VCCB 2.5V trasition at 200Mbps driving a load <15pF. 

Thank you

  • Hey Elisha,

    It's possible to test this using one of the EVMs listed on the product folder. Or this can be estimated using the following FAQ:

    There are several voltage nodes listed in the datasheet so finding one close to the values the customer is looking for shouldn't be difficult.